What are the best electrical practices in humid areas?
Electricity and water have never been compatible, and the design of an electrical installation in wet rooms, such as a bathroom, requires particular caution because they are more exposed to risks than other rooms in the home. The NF C 15-100 standard provides recommendations on this subject.
PROTECTION VOLUMES: A CONCERN FOR SAFETY
For the bathroom, the NF C 15-100 standard distinguishes different types of volume, each corresponding to a level of exposure:
- Volume 0: this is the area where water is received (bath or shower). No electrical equipment is allowed in this area.
- Volume 1: it is constituted by the zone in which the water is projected around volume 0, delimited by the edges of the shower tray and/or by a height of 2,25 m.
- Volume 2: it corresponds to a safety zone around the shower tray, on a distance of 60 cm beyond volume 1.
- The hidden volume: it is the space under the bathtub or the shower tray. No electrical equipment is allowed here (except for IPX4 products protected by a 30 mA differential switch, such as a whirlpool motor).
The rest of the bathroom is considered "out of volume".
Note: only fixed and permanent walls joined to the floor limit the volumes.
Volumes 0, 1 and 2
![practices-humid-areas](/sites/g/files/ocwmcr531/files/inline-images/EN-Bonnes-pratiques-electricite-et-pieces-humides-01-1440x670.jpg)
Volume 0: case of walk-in showers (without shower tray)
![practices-humid-areas](/sites/g/files/ocwmcr531/files/inline-images/EN-Bonnes-pratiques-electricite-et-pieces-humides-02-1440x350.jpg)
Hidden volume
![practices-humid-areas](/sites/g/files/ocwmcr531/files/inline-images/EN-Bonnes-pratiques-electricite-et-pieces-humides-03-1440x450.jpg)
WHICH EQUIPMENT IN WHICH VOLUME(S)?
The volumes defined by the NF C 15-100 standard determine the installation of electrical circuits and devices according to their protection measure.
Please note: the NF C 15-100 standard requires that all electrical circuits supplying a bathroom be protected by a 30 mA differential switch. In order for this switch to play its protective role, the pipes, metal masses and lighting in the bathroom must be connected to the ground.
![practices-humid-areas](/sites/g/files/ocwmcr531/files/inline-images/EN-Bonnes-pratiques-electricite-et-pieces-humides-04-1440x2600.jpg)